AKD PDMM and PCMM - File Naming Conventions
AKD PDMM and PCMM use only .IMG files.
File Contents
This .IMG file contains the Operating System (OS) and the KAS Runtime
In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time).
Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running (RT) software.
Usage
The contents of this .IMG file are used to update the AKD PDMM and PCMM from the web server interface.
File Format and Examples
AKD PDMM
|
Controller |
File Name Format |
Example File Name |
|---|---|---|
|
AKD PDMM |
KAS-PDMM-M-{Model-Code}-{Software-Version}.img
|
KAS-PDMM-M-K1EC-4.01.0.91992.img |
PCMM
|
Controller |
File Name Format |
Example File Name |
|---|---|---|
|
PCMM |
KAS-PCMM-M-{Model-Code}-{Software-Version}.img
|
KAS-PCMM-M-M2EC-4.01.0.91992.img |
Model Code
This table shows the specified model's CPU speed and number of cores.
|
Model Code |
CPU Speed |
Core |
|---|---|---|
|
KCEC and MCEC |
800 MHz |
Single |
|
K1EC and M1EC |
1.2 GHz |
Single |
|
M2EC |
1.2 GHz |
Dual |
See Also
- PCMM2G - File Naming Conventions
- AKD PDMM and PCMM - File Naming Conventions
- Operating System (OS) License Sources - File Naming Convention
- Operating System (OS) + KAS Runtime (RT) - File Naming Convention
- Recovery Operating System (OS) + KAS Runtime (RT) - File Naming Convention
- KAS Runtime (RT) Only - File Naming Convention
- Recover Using the Web server