Controller Backup and Restore

The Backup and Restore functions are used to replicate a Kollmorgen controller.

The controller data is replicated on these storage devices:

Backup

Backup is performed with one of these methods:

  • Use the web server.
  • Use the B3 Menu Button on the front of the controller.
    • See B3 Button Backup for more information.
    • PCMM2G: Currently does not support controller backup using the B3 menu button.

  • For a complete backup of both the controller and drive, use the Web Server backup.

Restore

Restoring information to the controller is performed with one of these methods. Both methods restore the controller (and AKD PDMM drive) with whatever was saved to the SD card.

Backup & Restore What?

AKD PDMM / PCMM

To/From
SD card
via B2/B3 buttons

 

AKD PDMM / PCMM

To/From
SD card
via Web server

PCMM2G

To/From
USB flash drive
via B2/B3 buttons

 

PCMM2G

To/From
USB flash drive
via Web server

Controller: Firmware

Controller: Network Configuration

Controller: PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events Application

Controller: Retain Variables

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Devices: Network Topology

EtherCAT Devices: AKD / AKD2G Drive Firmware

‡

EtherCAT Devices: AKD / AKD2G Drive Parameters

‡ Restore only

Data Transfer

  • The 7-segment display shows chasing light animation while the backup or restore is occurring.
    (repeats)
  • The Backup and Restore functions have an all-or-nothing behavior.
    • AKD PDMM / PCMM: If there is no SD card inserted, not enough space on the card, or if files are missing, nothing is copied and the 7-segment display shows an error code.
    • PCMM2G: If there is no USB flash drive inserted, not enough space on the USB, or if files are missing, nothing is copied and the 7-segment display shows an error code.
  • If files already exist on the SD card or USB flash drive (in the backup directory), they are deleted and replaced with the new backup configuration files.
    • The files on the controller are replaced with the SD card or USB flash drive files.

  • Do not modify the files on the SD card or USB flash drive.
    This could result in the restore function failing.


  • If there are multiple backup configurations, you must use one SD card or USB flash drive per backup configuration.