USB Flash Drive tab
-
This tab is only visible for PCMM2G controllers.
This tab is used to format the USB
"Universal Serial Bus"
USB is a serial bus standard to interface devices flash drive as FAT32.
-
- PCMM2G supports only one USB flash drive.
If a USB hub is used to expand the USB ports on the PCMM2G, use only a single USB flash drive in the hub.
-
- All data is erased from the USB flash drive.
The Format function cannot be performed while an application is running.
Figure 5-16: USB Flash Drive tab