View the Controller IP Address
The IP Address assigned to the controller is shown in the 7-segment display.
- The IP is shown at boot and can be accessed from the B3 Menu Button.
- The default IP address depends on the Rotary Switch RS1 position.
Example
-
-
The AKD PDMM and PCMM do not set (or show) an IP address without an attached network cable.
On the PCMM2G, if a network cable is not attached or no IP address is assigned, the controller shows an IP address of 0.0.0.0.