Change Controller's Password using SSH
This method is used to change the controller's root password using SSH.
- Log on through SSH
The Secure Shell Protocol (SSH) is a network protocol for secure data communication and remote command execution. SSH applications are based on a client–server architecture, connecting an SSH client instance with an SSH server.. - At the prompt, type passwd and press <Enter>.
- If prompted, enter the current password.
- In the next two prompts, enter the new password.
-
- AKD PDMM and PCMM use the root account.
PCMM2G uses the admin account.
AKD PDMM and PCMM: Change Password
# passwd changing password for root New password: Retype new password: #
PCMM2G: Change Password
kas-pcmm2g:~$ passwd Changing password for admin. Current password: New password: Retype new password: passwd: password updated successfully