Trace Zoom Feature

The zoom feature is used to magnify or reduce a portion of a trace. Two zoom modes are available:

Time zoom Used to expand/collapse the time-base in order to have a better view of the signal evolution through time.
This zoom operation updates the time-base value.
Amplitude zoom Used to have a better view of a part of a signal.
This zoom operation updates the amplitude & zero offset value

The zoom operations can be done:

  • By modifying the corresponding values by hand
  • By using the mouse wheel

For more details on setting the amplitude, zero offset and time-base values, refer to Setting Scale.

Mouse Shortcuts

Action Result
Scrolling up the mouse wheel Expands the time-base value
Scrolling down the mouse wheel Collapses the time-base value
Pressing the Ctrl key while scrolling up Makes the amplitude value greater
Pressing the Ctrl key while scrolling down Makes the amplitude value smaller

  • When performing an amplitude zoom, the zero offset is automatically set by the cursor position.