CAM Profile Switching
At pipe network start-up or when using the MLCamSwitch function block, a CAM block's output position is set to the output position of the initialized profile.
Example
- Assume:
- This profile is switched on.
- The present pipe network position is:
- 150 at the input of the CAM block.
- 50 at the output of the CAM block.
- Result:
- As the input to the CAM block increases or decreases, the CAM output value increases or decreases respectively.
- It will go through the modulo without a position jump.