EtherCAT Toolbar
Each icon in this toolbox has a brief explanation provided below in order to explain the functionality.
Icon | Name | Description |
---|---|---|
Online Configuration Mode |
This action is only available when the KAS Runtime In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running is connected with the target Controller.
|