ACTION#.CONDITIONVALUE
Description
ACTION#.CONDITIONVALUE defines the value used by ACTION#.CONDITION to test against the source. The range of this keyword depends on the value of ACTION#.SOURCE and ACTION#.CONDITION. Both must be set before setting the condition value. If ACTION#.CONDITION is modified, the range of the ACTION#.CONDITIONVALUE may change, and the value will return to default.
Some conditions do not require a condition value.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
Depends on ACTION#.SOURCE and ACTION#.CONDITION |
Default Value |
Depends on ACTION#.SOURCE and ACTION#.CONDITION |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
ACTION1.CONDITIONVALUE |
3902h |
01h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION2.CONDITIONVALUE |
3902h |
02h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION3.CONDITIONVALUE |
3902h |
03h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION4.CONDITIONVALUE |
3902h |
04h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION5.CONDITIONVALUE |
3902h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION6.CONDITIONVALUE |
3902h |
06h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION7.CONDITIONVALUE |
3902h |
07h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION8.CONDITIONVALUE |
3902h |
08h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION9.CONDITIONVALUE |
3902h |
09h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION10.CONDITIONVALUE |
3902h |
0ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION11.CONDITIONVALUE |
3902h |
0bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION12.CONDITIONVALUE |
3902h |
0ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION13.CONDITIONVALUE |
3902h |
0dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION14.CONDITIONVALUE |
3902h |
0eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION15.CONDITIONVALUE |
3902h |
0fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION16.CONDITIONVALUE |
3902h |
10h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION17.CONDITIONVALUE |
3902h |
11h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION18.CONDITIONVALUE |
3902h |
12h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION19.CONDITIONVALUE |
3902h |
13h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION20.CONDITIONVALUE |
3902h |
14h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION21.CONDITIONVALUE |
3902h |
15h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION22.CONDITIONVALUE |
3902h |
16h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION23.CONDITIONVALUE |
3902h |
17h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION24.CONDITIONVALUE |
3902h |
18h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION25.CONDITIONVALUE |
3902h |
19h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION26.CONDITIONVALUE |
3902h |
1ah |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION27.CONDITIONVALUE |
3902h |
1bh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION28.CONDITIONVALUE |
3902h |
1ch |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION29.CONDITIONVALUE |
3902h |
1dh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION30.CONDITIONVALUE |
3902h |
1eh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION31.CONDITIONVALUE |
3902h |
1fh |
Signed32 |
- |
1000:1 |
Read/Write |
No |
ACTION32.CONDITIONVALUE |
3902h |
20h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
ACTION1.CONDITIONVALUE |
40300 |
9D6C |
Signed32 |
Read/Write |
- |
ACTION2.CONDITIONVALUE |
40301 |
9D6D |
Signed32 |
Read/Write |
- |
ACTION3.CONDITIONVALUE |
40302 |
9D6E |
Signed32 |
Read/Write |
- |
ACTION4.CONDITIONVALUE |
40303 |
9D6F |
Signed32 |
Read/Write |
- |
ACTION5.CONDITIONVALUE |
40304 |
9D70 |
Signed32 |
Read/Write |
- |
ACTION6.CONDITIONVALUE |
40305 |
9D71 |
Signed32 |
Read/Write |
- |
ACTION7.CONDITIONVALUE |
40306 |
9D72 |
Signed32 |
Read/Write |
- |
ACTION8.CONDITIONVALUE |
40307 |
9D73 |
Signed32 |
Read/Write |
- |
ACTION9.CONDITIONVALUE |
40308 |
9D74 |
Signed32 |
Read/Write |
- |
ACTION10.CONDITIONVALUE |
40309 |
9D75 |
Signed32 |
Read/Write |
- |
ACTION11.CONDITIONVALUE |
40310 |
9D76 |
Signed32 |
Read/Write |
- |
ACTION12.CONDITIONVALUE |
40311 |
9D77 |
Signed32 |
Read/Write |
- |
ACTION13.CONDITIONVALUE |
40312 |
9D78 |
Signed32 |
Read/Write |
- |
ACTION14.CONDITIONVALUE |
40313 |
9D79 |
Signed32 |
Read/Write |
- |
ACTION15.CONDITIONVALUE |
40314 |
9D7A |
Signed32 |
Read/Write |
- |
ACTION16.CONDITIONVALUE |
40315 |
9D7B |
Signed32 |
Read/Write |
- |
ACTION17.CONDITIONVALUE |
40316 |
9D7C |
Signed32 |
Read/Write |
- |
ACTION18.CONDITIONVALUE |
40317 |
9D7D |
Signed32 |
Read/Write |
- |
ACTION19.CONDITIONVALUE |
40318 |
9D7E |
Signed32 |
Read/Write |
- |
ACTION20.CONDITIONVALUE |
40319 |
9D7F |
Signed32 |
Read/Write |
- |
ACTION21.CONDITIONVALUE |
40320 |
9D80 |
Signed32 |
Read/Write |
- |
ACTION22.CONDITIONVALUE |
40321 |
9D81 |
Signed32 |
Read/Write |
- |
ACTION23.CONDITIONVALUE |
40322 |
9D82 |
Signed32 |
Read/Write |
- |
ACTION24.CONDITIONVALUE |
40323 |
9D83 |
Signed32 |
Read/Write |
- |
ACTION25.CONDITIONVALUE |
40324 |
9D84 |
Signed32 |
Read/Write |
- |
ACTION26.CONDITIONVALUE |
40325 |
9D85 |
Signed32 |
Read/Write |
- |
ACTION27.CONDITIONVALUE |
40326 |
9D86 |
Signed32 |
Read/Write |
- |
ACTION28.CONDITIONVALUE |
40327 |
9D87 |
Signed32 |
Read/Write |
- |
ACTION29.CONDITIONVALUE |
40328 |
9D88 |
Signed32 |
Read/Write |
- |
ACTION30.CONDITIONVALUE |
40329 |
9D89 |
Signed32 |
Read/Write |
- |
ACTION31.CONDITIONVALUE |
40330 |
9D8A |
Signed32 |
Read/Write |
- |
ACTION32.CONDITIONVALUE |
40331 |
9D8B |
Signed32 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
ACTION1.CONDITIONVALUE |
40300 |
Float |
Read/Write |
- |
ACTION2.CONDITIONVALUE |
40301 |
Float |
Read/Write |
- |
ACTION3.CONDITIONVALUE |
40302 |
Float |
Read/Write |
- |
ACTION4.CONDITIONVALUE |
40303 |
Float |
Read/Write |
- |
ACTION5.CONDITIONVALUE |
40304 |
Float |
Read/Write |
- |
ACTION6.CONDITIONVALUE |
40305 |
Float |
Read/Write |
- |
ACTION7.CONDITIONVALUE |
40306 |
Float |
Read/Write |
- |
ACTION8.CONDITIONVALUE |
40307 |
Float |
Read/Write |
- |
ACTION9.CONDITIONVALUE |
40308 |
Float |
Read/Write |
- |
ACTION10.CONDITIONVALUE |
40309 |
Float |
Read/Write |
- |
ACTION11.CONDITIONVALUE |
40310 |
Float |
Read/Write |
- |
ACTION12.CONDITIONVALUE |
40311 |
Float |
Read/Write |
- |
ACTION13.CONDITIONVALUE |
40312 |
Float |
Read/Write |
- |
ACTION14.CONDITIONVALUE |
40313 |
Float |
Read/Write |
- |
ACTION15.CONDITIONVALUE |
40314 |
Float |
Read/Write |
- |
ACTION16.CONDITIONVALUE |
40315 |
Float |
Read/Write |
- |
ACTION17.CONDITIONVALUE |
40316 |
Float |
Read/Write |
- |
ACTION18.CONDITIONVALUE |
40317 |
Float |
Read/Write |
- |
ACTION19.CONDITIONVALUE |
40318 |
Float |
Read/Write |
- |
ACTION20.CONDITIONVALUE |
40319 |
Float |
Read/Write |
- |
ACTION21.CONDITIONVALUE |
40320 |
Float |
Read/Write |
- |
ACTION22.CONDITIONVALUE |
40321 |
Float |
Read/Write |
- |
ACTION23.CONDITIONVALUE |
40322 |
Float |
Read/Write |
- |
ACTION24.CONDITIONVALUE |
40323 |
Float |
Read/Write |
- |
ACTION25.CONDITIONVALUE |
40324 |
Float |
Read/Write |
- |
ACTION26.CONDITIONVALUE |
40325 |
Float |
Read/Write |
- |
ACTION27.CONDITIONVALUE |
40326 |
Float |
Read/Write |
- |
ACTION28.CONDITIONVALUE |
40327 |
Float |
Read/Write |
- |
ACTION29.CONDITIONVALUE |
40328 |
Float |
Read/Write |
- |
ACTION30.CONDITIONVALUE |
40329 |
Float |
Read/Write |
- |
ACTION31.CONDITIONVALUE |
40330 |
Float |
Read/Write |
- |
ACTION32.CONDITIONVALUE |
40331 |
Float |
Read/Write |
- |