ACTION#.TASKPARAM

Description

Some tasks require a Task Param value to specify what is acted upon. ACTION#.TASK must be set before ACTION#.TASKPARAM. If ACTION#.TASK is modified, then the range and units of ACTION#.TASKPARAM may be modified, and the value will be defaulted.

Not all tasks require a task param.

Example

This example shows an action which starts a motion task 4 on AXIS1

>> ACTION1.TASK = 5 (Launch motion task)

>> ACTION1.TASKID = 1 (AXIS1)

>> ACTION1.TASKPARAM = 4

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

Depends on ACTION#.TASK

Default Value

Depends on ACTION#.TASK

Data Type

Float

Stored in Non-Volatile Memory

Yes

Task Parameter Values for Certain Tasks

Task: Set the Command Source and Op-Mode for an axis.

Command Source and Op-mode combination Value
Service/TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist 0
Service/Velocity 1
Service/Position 2
Service/No Change 9
FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design/Torque 10
Fieldbus/Velocity 11
Fieldbus/Position 12
Fieldbus/No Change 19
Electronic Gearing/Position 22
Analog/Torque 30
Analog/Velocity 31
Analog/Position 32
Analog/No Change 39
No Change/Torque 90
No Change/Velocity 91
No Change/Position 92

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

ACTION1.TASKPARAM

3909h

01h

Signed32

-

1000:1

Read/Write

No

ACTION2.TASKPARAM

3909h

02h

Signed32

-

1000:1

Read/Write

No

ACTION3.TASKPARAM

3909h

03h

Signed32

-

1000:1

Read/Write

No

ACTION4.TASKPARAM

3909h

04h

Signed32

-

1000:1

Read/Write

No

ACTION5.TASKPARAM

3909h

05h

Signed32

-

1000:1

Read/Write

No

ACTION6.TASKPARAM

3909h

06h

Signed32

-

1000:1

Read/Write

No

ACTION7.TASKPARAM

3909h

07h

Signed32

-

1000:1

Read/Write

No

ACTION8.TASKPARAM

3909h

08h

Signed32

-

1000:1

Read/Write

No

ACTION9.TASKPARAM

3909h

09h

Signed32

-

1000:1

Read/Write

No

ACTION10.TASKPARAM

3909h

0ah

Signed32

-

1000:1

Read/Write

No

ACTION11.TASKPARAM

3909h

0bh

Signed32

-

1000:1

Read/Write

No

ACTION12.TASKPARAM

3909h

0ch

Signed32

-

1000:1

Read/Write

No

ACTION13.TASKPARAM

3909h

0dh

Signed32

-

1000:1

Read/Write

No

ACTION14.TASKPARAM

3909h

0eh

Signed32

-

1000:1

Read/Write

No

ACTION15.TASKPARAM

3909h

0fh

Signed32

-

1000:1

Read/Write

No

ACTION16.TASKPARAM

3909h

10h

Signed32

-

1000:1

Read/Write

No

ACTION17.TASKPARAM

3909h

11h

Signed32

-

1000:1

Read/Write

No

ACTION18.TASKPARAM

3909h

12h

Signed32

-

1000:1

Read/Write

No

ACTION19.TASKPARAM

3909h

13h

Signed32

-

1000:1

Read/Write

No

ACTION20.TASKPARAM

3909h

14h

Signed32

-

1000:1

Read/Write

No

ACTION21.TASKPARAM

3909h

15h

Signed32

-

1000:1

Read/Write

No

ACTION22.TASKPARAM

3909h

16h

Signed32

-

1000:1

Read/Write

No

ACTION23.TASKPARAM

3909h

17h

Signed32

-

1000:1

Read/Write

No

ACTION24.TASKPARAM

3909h

18h

Signed32

-

1000:1

Read/Write

No

ACTION25.TASKPARAM

3909h

19h

Signed32

-

1000:1

Read/Write

No

ACTION26.TASKPARAM

3909h

1ah

Signed32

-

1000:1

Read/Write

No

ACTION27.TASKPARAM

3909h

1bh

Signed32

-

1000:1

Read/Write

No

ACTION28.TASKPARAM

3909h

1ch

Signed32

-

1000:1

Read/Write

No

ACTION29.TASKPARAM

3909h

1dh

Signed32

-

1000:1

Read/Write

No

ACTION30.TASKPARAM

3909h

1eh

Signed32

-

1000:1

Read/Write

No

ACTION31.TASKPARAM

3909h

1fh

Signed32

-

1000:1

Read/Write

No

ACTION32.TASKPARAM

3909h

20h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

ACTION1.TASKPARAM

41000

A028

Signed32

Read/Write

-

ACTION2.TASKPARAM

41001

A029

Signed32

Read/Write

-

ACTION3.TASKPARAM

41002

A02A

Signed32

Read/Write

-

ACTION4.TASKPARAM

41003

A02B

Signed32

Read/Write

-

ACTION5.TASKPARAM

41004

A02C

Signed32

Read/Write

-

ACTION6.TASKPARAM

41005

A02D

Signed32

Read/Write

-

ACTION7.TASKPARAM

41006

A02E

Signed32

Read/Write

-

ACTION8.TASKPARAM

41007

A02F

Signed32

Read/Write

-

ACTION9.TASKPARAM

41008

A030

Signed32

Read/Write

-

ACTION10.TASKPARAM

41009

A031

Signed32

Read/Write

-

ACTION11.TASKPARAM

41010

A032

Signed32

Read/Write

-

ACTION12.TASKPARAM

41011

A033

Signed32

Read/Write

-

ACTION13.TASKPARAM

41012

A034

Signed32

Read/Write

-

ACTION14.TASKPARAM

41013

A035

Signed32

Read/Write

-

ACTION15.TASKPARAM

41014

A036

Signed32

Read/Write

-

ACTION16.TASKPARAM

41015

A037

Signed32

Read/Write

-

ACTION17.TASKPARAM

41016

A038

Signed32

Read/Write

-

ACTION18.TASKPARAM

41017

A039

Signed32

Read/Write

-

ACTION19.TASKPARAM

41018

A03A

Signed32

Read/Write

-

ACTION20.TASKPARAM

41019

A03B

Signed32

Read/Write

-

ACTION21.TASKPARAM

41020

A03C

Signed32

Read/Write

-

ACTION22.TASKPARAM

41021

A03D

Signed32

Read/Write

-

ACTION23.TASKPARAM

41022

A03E

Signed32

Read/Write

-

ACTION24.TASKPARAM

41023

A03F

Signed32

Read/Write

-

ACTION25.TASKPARAM

41024

A040

Signed32

Read/Write

-

ACTION26.TASKPARAM

41025

A041

Signed32

Read/Write

-

ACTION27.TASKPARAM

41026

A042

Signed32

Read/Write

-

ACTION28.TASKPARAM

41027

A043

Signed32

Read/Write

-

ACTION29.TASKPARAM

41028

A044

Signed32

Read/Write

-

ACTION30.TASKPARAM

41029

A045

Signed32

Read/Write

-

ACTION31.TASKPARAM

41030

A046

Signed32

Read/Write

-

ACTION32.TASKPARAM

41031

A047

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

ACTION1.TASKPARAM

41000

Float

Read/Write

-

ACTION2.TASKPARAM

41001

Float

Read/Write

-

ACTION3.TASKPARAM

41002

Float

Read/Write

-

ACTION4.TASKPARAM

41003

Float

Read/Write

-

ACTION5.TASKPARAM

41004

Float

Read/Write

-

ACTION6.TASKPARAM

41005

Float

Read/Write

-

ACTION7.TASKPARAM

41006

Float

Read/Write

-

ACTION8.TASKPARAM

41007

Float

Read/Write

-

ACTION9.TASKPARAM

41008

Float

Read/Write

-

ACTION10.TASKPARAM

41009

Float

Read/Write

-

ACTION11.TASKPARAM

41010

Float

Read/Write

-

ACTION12.TASKPARAM

41011

Float

Read/Write

-

ACTION13.TASKPARAM

41012

Float

Read/Write

-

ACTION14.TASKPARAM

41013

Float

Read/Write

-

ACTION15.TASKPARAM

41014

Float

Read/Write

-

ACTION16.TASKPARAM

41015

Float

Read/Write

-

ACTION17.TASKPARAM

41016

Float

Read/Write

-

ACTION18.TASKPARAM

41017

Float

Read/Write

-

ACTION19.TASKPARAM

41018

Float

Read/Write

-

ACTION20.TASKPARAM

41019

Float

Read/Write

-

ACTION21.TASKPARAM

41020

Float

Read/Write

-

ACTION22.TASKPARAM

41021

Float

Read/Write

-

ACTION23.TASKPARAM

41022

Float

Read/Write

-

ACTION24.TASKPARAM

41023

Float

Read/Write

-

ACTION25.TASKPARAM

41024

Float

Read/Write

-

ACTION26.TASKPARAM

41025

Float

Read/Write

-

ACTION27.TASKPARAM

41026

Float

Read/Write

-

ACTION28.TASKPARAM

41027

Float

Read/Write

-

ACTION29.TASKPARAM

41028

Float

Read/Write

-

ACTION30.TASKPARAM

41029

Float

Read/Write

-

ACTION31.TASKPARAM

41030

Float

Read/Write

-

ACTION32.TASKPARAM

41031

Float

Read/Write

-