AXIS#.BODE.CHIRP​.ENDFREQ

Description

AXIS#.BODE.CHIRP.ENDFREQ sets the ending frequency for the chirp excitation.

Example

Setting up a chirp excitation source of 0.2 A from 0.1 Hz to 1000 Hz over a period of 1 second:

--> AXIS1.BODE.INJECTPOINT 1
--> AXIS1.BODE.IAMP 0.2
--> AXIS1.BODE.CHIRP.STARTFREQ 0.1
--> AXIS1.BODE.CHIRP.ENDFREQ 1000
--> AXIS1.BODE.CHIRP.TIME 1
--> AXIS1.BODE.MODE 6

Versions

Action Version Notes
Implemented 02-09-04-000

General Information

Type

Read/Write

Description

Sets the end frequency of the chirp excitation.

Units Hz

Range

0.1 to 8,000 Hz

Default Value

1000 Hz

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.