AXIS#.BODE.CHIRP​.STARTFREQ

Description

AXIS#.BODE.CHIRP.STARTFREQ sets the start frequency for the chirp excitation

Example

Setting up a chirp excitation source of 0.2 A from 0.1 Hz to 1000 Hz over a period of 1 second:

--> AXIS1.BODE.INJECTPOINT 1
--> AXIS1.BODE.IAMP 0.2
--> AXIS1.BODE.CHIRP.STARTFREQ 0.1
--> AXIS1.BODE.CHIRP.ENDFREQ 1000
--> AXIS1.BODE.CHIRP.TIME 1
--> AXIS1.BODE.MODE 6

Versions

Action Version Notes
Implemented 02-09-04-000

General Information

Type

Read/Write

Description Sets the start frequency of the chirp excitation.
Units Hz
Range 0.1 to 8,000 Hz
Default Value 0.1 Hz
Data Type Float
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.