AXIS#.IL.KP
Description
AXIS#.IL
"Instruction List"
This is a low-level language and resembles assembly.KP is used to read the proportional gain of the PI-loop that controls the q-component of the current.
The value is Read-Only, and is changed by modifying the current loop bandwidth
In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz setting (AXIS#.IL.BW).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
V/A |
|
Range |
0 to 2,000 V/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.KP |
500ah |
02h |
Unsigned32 |
- |
1000:1 |
Read only |
No |
|
AXIS2.IL.KP |
510ah |
02h |
Unsigned32 |
- |
1000:1 |
Read only |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.IL.KP |
5819 |
16BB |
Unsigned32 |
Read Only |
- |
|
AXIS2.IL.KP |
71355 |
116B |
Unsigned32 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.KP |
5819 |
Float |
Read Only |
- |