AXIS#.IL.LIMITN

Description

This parameter sets the negative user limit clamp value of the torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

Negative drive peak current (IPEAK) to 0 A

Default Value

Negative drive peak current (IPEAK)

Data Type

Float

See Also

AXIS#.IL.LIMITP

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.IL.LIMITN

500ah

05h

Signed32

-

1000:1

Read/Write

No

AXIS2.IL.LIMITN

510ah

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.LIMITN

5813

16B5

Signed32

Read/Write

-

AXIS2.IL.LIMITN

71349

116B

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.LIMITN

5813

Float

Read/Write

-