AXIS#.MOTOR.BRAKEPOWERDELAY
Description
Time to wait after applying full voltage before dropping to low voltage when AXIS#.MOTOR.BRAKEPOWERSAVING = 1.
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.4 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Milliseconds |
|
Range |
0 to 2000 |
|
Default Value |
150 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.BRAKEPOWERDELAY |
500bh |
24h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
AXIS2.MOTOR.BRAKEPOWERDELAY |
510bh |
24h |
Unsigned16 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.MOTOR.BRAKEPOWERDELAY |
6238 |
185E |
Unsigned16 |
Read Only |
- |
|
AXIS2.MOTOR.BRAKEPOWERDELAY |
71774 |
1185 |
Unsigned16 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.BRAKEPOWERDELAY |
6238 |
Unsigned16 |
Read Only |
- |