AXIS#.MOTOR.LQLL

Description

This parameter is the motor line-to-line quadrature (torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist producing) axis inductance.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mH

Range

1 to 232 mH

Default Value

4

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.MOTOR.LQLL

500bh

14h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.LQLL

510bh

14h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.LQLL

6209

1841

Unsigned32

Read Only

-

AXIS2.MOTOR.LQLL

71745

1184

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.LQLL

6209

Float

Read Only

-