AXIS#.MOTOR.TEMPFAULT
Description
This parameter is used to configure the motor temperature fault level as a resistance threshold of the motor thermal sensor
A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.
A zero value prevents temperature faults from being reported.
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET=1 and motor memory version is 0.3 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
Context
For more information see Motor and Motor Temperature View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Ω |
|
Range |
0 to 2,000,000,000 Ω |
|
Default Value |
2000 |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.TEMPFAULT |
500bh |
1dh |
Unsigned32 |
- |
- |
Read/Write |
No |
|
AXIS2.MOTOR.TEMPFAULT |
510bh |
1dh |
Unsigned32 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.MOTOR.TEMPFAULT |
6218 |
184A |
Unsigned32 |
Read Only |
- |
|
AXIS2.MOTOR.TEMPFAULT |
71754 |
1184 |
Unsigned32 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.TEMPFAULT |
6218 |
Unsigned32 |
Read Only |
- |