AXIS#.MOTOR.VRATED
Description
This parameter configures the drive for the rated velocity of the induction motor as indicated on the nameplate. AXIS#.MOTOR.VRATED is used to calculate the constant volts per Hertz characteristics of the drive and motor.
-
-
This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.
Context
For more information see Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
1200 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.VRATED |
500bh |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.MOTOR.VRATED |
510bh |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.MOTOR.VRATED |
6227 |
1853 |
Signed32 |
Read/Write |
Velocity |
|
AXIS2.MOTOR.VRATED |
71763 |
1185 |
Signed32 |
Read/Write |
Velocity |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.VRATED |
6227 |
Float |
Read/Write |
Velocity |