AXIS#.OBS.BW

Description

AXIS#.OBS.BW sets the frequency at which the observer starts being the dominant component in the velocity signal.

Versions

Action Version Notes
Implemented 02-04-03-000  

General Information

Type

Read/Write

Units

Hz

Range

1 to 8,000.000

Default Value

500

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.OBS.BW

5017h

01h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.OBS.BW

5117h

01h

Unsigned32

-

1000:1

Read/Write

No