AXIS#.WS.CHECKV
Description
This parameter sets the velocity threshold which has to be exceeded to activate commutation monitoring.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
||
|
Units |
Rotary: RPM See Velocity Units for details. |
||
|
Range |
Depends on units. See Velocity Range for details. |
||
|
Default Value |
N/A |
||
|
Data Type |
Float |
||
|
Stored in Non-Volatile Memory |
Yes |
||
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
AXIS1.WS.CHECKV |
5013h |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
AXIS2.WS.CHECKV |
5113h |
0bh |
Signed32 |
Velocity |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
AXIS1.WS.CHECKV |
6716 |
1A3C |
Signed32 |
Read/Write |
Velocity |
|
AXIS2.WS.CHECKV |
72252 |
11A3 |
Signed32 |
Read/Write |
Velocity |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.WS.CHECKV |
6716 |
Float |
Read/Write |
Velocity |