AXIS#.ZEROACC

Description

AXIS#.ZEROACC is the acceleration threshold for the motor to be considered at zero velocity.

If AXIS#.ZEROACC is equal to 0, acceleration will not be included in determining zero velocity. If AXIS#.ZEROACC is greater than zero, it will be included.

Versions

Action Version Notes
Implemented 02-04-01-000

 

General Information

Type

Read/Write

Units

Rotary: RPMClosed "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2, (custom units)/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value

0 RPM

Depends on units. See Acceleration Units for details.

Data Type

Float

Stored in Non Volatile Memory Yes

Variants Supported

All variants supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.ZEROACC

5002h

05h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.ZEROACC

5102h

05h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.ZEROACC

5031

13A7

Unsigned32

Read/Write

Acceleration

AXIS2.ZEROACC

70567

113A

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.ZEROACC

5031

Float

Read/Write

Acceleration