AXIS#.ZEROV
Description
AXIS#.ZEROV is the velocity threshold for the motor to be considered at zero velocity.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
|
Renamed from AXIS#.DISVTHRESH | 02-03-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
5 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
AXIS1.ZEROV |
5002h |
04h |
Signed32 |
Velocity |
- |
Read/Write |
No |
AXIS2.ZEROV |
5102h |
04h |
Signed32 |
Velocity |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.ZEROV |
5002 |
138A |
Signed32 |
Read/Write |
Velocity |
AXIS2.ZEROV |
70538 |
1138 |
Signed32 |
Read/Write |
Velocity |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.ZEROV |
5002 |
Float |
Read/Write |
Velocity |