AXIS#.SETUPREQBITS

Description

AXIS#.SETUPREQBITS is a bit-field that returns the set of parameters that needs to be set up before the drive can be enabled. The drive can only be enabled when this parameter returns 0.

The following table lists the parameters which require setup for each motor type.

Index Bit Default Value Induction Motor V/f Open LoopClosed A positioning technique, typically utilizing stepper motors, in which the controller issues a sequence of commands to the motor without an absolute means of detecting if the move has been made. When the load and move velocity and acceleration are appropriately defined, open loop positioning is capable of extended operation without losing steps. (MOTOR.TYPE 2) Induction Motor Closed LoopClosed The use of feedback devices (encoders, resolvers, interferometers, etc.) to allow a motor to position a user payload accurately. (MOTOR.TYPE 4) ) Interior Permanent Magnet (MOTOR.TYPE 6) Sensorless Permanent Magnet (MOTOR.TYPE 10)
AXIS#.MOTOR.IPEAK 0 2 Arms √ √ √ √
AXIS#.MOTOR.ICONT 1 1 Arms √ √ √ √
AXIS#.MOTOR.POLES 3 6 √ √ √ √
AXIS#.MOTOR.LDLL 6 4 mH - √ √ √
AXIS#.MOTOR.LQLL 7 4 mH - √ √ √
AXIS#.MOTOR.KE 8 20 - - √ -
AXIS#.MOTOR.IMTR 9 100 ms - √ - -
AXIS#.MOTOR.IMID 10 0 Arms - √ - -
AXIS#.MOTOR.VOLTRATED 11 230 VrmsClosed rms stands for root mean square (also known as the quadratic mean) √ - - -
AXIS#.MOTOR.VRATED 12 1200 RPMClosed "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component √ - - -
AXIS#.MOTOR.LISAT 13 1000 x AXIS#.IPEAK - - √ -
AXIS#.MOTOR.PHSADVK1 14 0 - - √ -
AXIS#.MOTOR.PHSADVK2 15 0 - - √ -
AXIS#.MOTOR.IDMAX 16 1 Arms - - √ -
AXIS#.MOTOR.PITCH 17 32 mm - - - -
AXIS#.MOTOR.VOLTMAX 18 480 Vrms - - √ -

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer (bit-field)

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.SETUPREQBITS

5017

1399

Unsigned32

Read Only

-

AXIS2.SETUPREQBITS

70553

1139

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.SETUPREQBITS

5017

Unsigned32

Read Only

-

Related Topics

AXIS#.SETUPREQLIST, AXIS#.MOTOR.AUTOSET