AXIS#.STOP

Description

This command stops drive motion. In torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist and velocity modes, the command value will immediately be set to 0. In position mode, the axis will decelerate to a full stop. If the position command is from a gearing master, the drive will cancel gearing and decelerate to a stop. This command has no effect if the command source is an analog input.

If the command values are coming from a fieldbus master, the stop may be immediately overwritten by a new fieldbus command. Use a controlled stop input or disable command to ensure a stop.

The following table defines the behavior of AXIS#.STOP:

Cmdsource Opmode Subopmode Deceleration ramp defined by:
Service TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist - AXIS#.ILClosed "Instruction List" This is a low-level language and resembles assembly.CMD = 0
Velocity - AXIS#.SM.DEC and AXIS#.SM.DEC 
Position Service motion AXIS#.SM.DEC and AXIS#.SM.DEC 
Motion tasking AXIS#.MT.DEC
HomingClosed The Homing procedure allows, based on a position measurement, to set a position offset to the motor in order to ensure it is physically at the home position AXIS#.HOME.DEC
FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Torque - Command has no effect.
Velocity
Position
Electronic Gearing Position - AXIS#.GEAR.DECMAX
Analog Torque - Command has no effect.
Velocity
Position

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.STOP

5016

1398

Unsigned8

Read/Write

-

AXIS2.STOP

70552

1139

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.STOP

5016

Unsigned8

Read/Write

-