BRAKE#.AXIS
Description
Sets which axis will control the brake.
Value | Description |
---|---|
0 | Not used |
1 | Controlled by Axis 1. |
2 | Controlled by Axis 2. |
Examples
Context
For more information see Brake.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 2 |
Default Value |
Depends on Brake and Axis number: BRAKE1 defaults to 1. BRAKE2 defaults to 2 on multi-axis drives and 0 on single-axis drives. |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
BRAKE1.AXIS |
3012h |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
BRAKE2.AXIS |
3012h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
BRAKE1.AXIS |
3100 |
C1C |
Unsigned8 |
Read/Write |
- |
BRAKE2.AXIS |
3101 |
C1D |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
BRAKE1.AXIS |
3100 |
Unsigned8 |
Read/Write |
- |
BRAKE2.AXIS |
3101 |
Unsigned8 |
Read/Write |
- |