DIO#.DIR
Description
Sets or whether the bi-directional IO is an input or output.
Value | Description |
---|---|
0 | The bi-directional IO is treated as an input signal |
1 | The bi-directional IO is treated as an output signal |
Examples
Context
For more information see Digital Inputs and Outputs.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 0 to 1 |
Default Value | 0 (input) |
Data Type | Integer |
See Also | |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
DIO1.DIR |
368ah |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
DIO2.DIR |
368bh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
DIO3.DIR |
368ch |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
DIO4.DIR |
368dh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
DIO5.DIR |
368eh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
DIO6.DIR |
368fh |
01h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
DIO1.DIR |
22050 |
5622 |
Unsigned8 |
Read/Write |
- |
DIO2.DIR |
22051 |
5623 |
Unsigned8 |
Read/Write |
- |
DIO3.DIR |
22052 |
5624 |
Unsigned8 |
Read/Write |
- |
DIO4.DIR |
22053 |
5625 |
Unsigned8 |
Read/Write |
- |
DIO5.DIR |
22054 |
5626 |
Unsigned8 |
Read/Write |
- |
DIO6.DIR |
22055 |
5627 |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
DIO1.DIR |
22050 |
Unsigned8 |
Read/Write |
- |
DIO2.DIR |
22051 |
Unsigned8 |
Read/Write |
- |
DIO3.DIR |
22052 |
Unsigned8 |
Read/Write |
- |
DIO4.DIR |
22053 |
Unsigned8 |
Read/Write |
- |
DIO5.DIR |
22054 |
Unsigned8 |
Read/Write |
- |
DIO6.DIR |
22055 |
Unsigned8 |
Read/Write |
- |