FB#.BITS
Description
Specifies the number of BiSS "Bi-directional Serial Synchronous interface" An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder sensor A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer (position) bits for the BiSS encoder in use when used for linear motors. The required value for this parameter is provided by the feedback device A process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position manufacturer for the particular device being used.
Context
Only used for when FB#.MECHTYPE is linear and identified feedback is BiSS. See Feedback # View.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
position bits |
Range |
0 to 64 |
Default Value |
26 |
Data Type |
Integer |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
FB1.BITS |
3500h |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
FB2.BITS |
3501h |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
FB3.BITS |
3502h |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
FB4.BITS |
3503h |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
FB5.BITS |
3504h |
06h |
Unsigned16 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
FB1.BITS |
30400 |
76C0 |
Unsigned16 |
Read/Write |
- |
FB2.BITS |
30401 |
76C1 |
Unsigned16 |
Read/Write |
- |
FB3.BITS |
30402 |
76C2 |
Unsigned16 |
Read/Write |
- |
FB4.BITS |
30403 |
76C3 |
Unsigned16 |
Read/Write |
- |
FB5.BITS |
30404 |
76C4 |
Unsigned16 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
FB1.BITS |
30400 |
Unsigned16 |
Read/Write |
- |
FB2.BITS |
30401 |
Unsigned16 |
Read/Write |
- |
FB3.BITS |
30402 |
Unsigned16 |
Read/Write |
- |
FB4.BITS |
30403 |
Unsigned16 |
Read/Write |
- |
FB5.BITS |
30404 |
Unsigned16 |
Read/Write |
- |