FB#.RESREFPHASE
Description
This parameter sets the electrical degrees of phase lag in the resolver.
See the motor resolver datasheet for the value for this parameter.
Context
See Feedback # View.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
electrical degrees |
|
Range |
-180 to 180° |
|
Default Value |
-2° |
|
Data Type |
Float |
|
See Also |
N/A |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
FB1.RESREFPHASE |
3500h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
FB2.RESREFPHASE |
3501h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
FB3.RESREFPHASE |
3502h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
FB4.RESREFPHASE |
3503h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
FB5.RESREFPHASE |
3504h |
05h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
FB1.RESREFPHASE |
30160 |
75D0 |
Signed32 |
Read/Write |
- |
|
FB2.RESREFPHASE |
30161 |
75D1 |
Signed32 |
Read/Write |
- |
|
FB3.RESREFPHASE |
30162 |
75D2 |
Signed32 |
Read/Write |
- |
|
FB4.RESREFPHASE |
30163 |
75D3 |
Signed32 |
Read/Write |
- |
|
FB5.RESREFPHASE |
30164 |
75D4 |
Signed32 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.RESREFPHASE |
30160 |
Float |
Read/Write |
- |
|
FB2.RESREFPHASE |
30161 |
Float |
Read/Write |
- |
|
FB3.RESREFPHASE |
30162 |
Float |
Read/Write |
- |
|
FB4.RESREFPHASE |
30163 |
Float |
Read/Write |
- |
|
FB5.RESREFPHASE |
30164 |
Float |
Read/Write |
- |