FB#.SIGNALSIN
Description
This parameter returns the measured analog sine channel signal of a connected resolver or sine/cosine encoder.
This parameter is only available on the following encoder types:
- Sine Encoder with Halls
- Sine Encoder without Halls
- EnDat Analog
- Resolver
- HIPERFACE
- BiSS
"Bi-directional Serial Synchronous interface"
An open-source communication protocol for feedback devices. With BiSS, all of the computation for interpolation in regard to position occurs on the ASIC directly in the encoder-B with SinCos
These commands are not recordable on FB1 and FB2.
For recording on FB1 and FB2, see FB#.MONITOR#.SOURCE and FB#.MONITOR#.DATA.
Examples
Usage
The sine signal measurement can be used to detect if a sine/cosine encoder was commissioned correctly.
Code
--> FB3.SIGNALSIN
0.423 [V]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-02-000 |
General Information
|
Type |
Read Only |
|
Units |
V |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
| Stored in Non-Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
FB1.SIGNALSIN |
30300 |
765C |
Signed32 |
Read Only |
- |
|
FB2.SIGNALSIN |
30301 |
765D |
Signed32 |
Read Only |
- |
|
FB3.SIGNALSIN |
30302 |
765E |
Signed32 |
Read Only |
- |
|
FB4.SIGNALSIN |
30303 |
765F |
Signed32 |
Read Only |
- |
|
FB5.SIGNALSIN |
30304 |
7660 |
Signed32 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.SIGNALSIN |
30300 |
Float |
Read Only |
- |
|
FB2.SIGNALSIN |
30301 |
Float |
Read Only |
- |
|
FB3.SIGNALSIN |
30302 |
Float |
Read Only |
- |
|
FB4.SIGNALSIN |
30303 |
Float |
Read Only |
- |
|
FB5.SIGNALSIN |
30304 |
Float |
Read Only |
- |
Related Topics