GANTRY.PL.ERRFTHRESH
Description
This parameter sets the maximum position error. If the position error GANTRY.PL.ERR is larger than GANTRY.PL.ERRFTHRESH then the drive generates a fault. If GANTRY.PL.ERRFTHRESH is set to 0, the maximum position error is ignored.
-
- Replace with note text.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-02-000 |
General Information
| Type | Read/Write |
| Description | Sets the maximum position error for Gantry Mode |
| Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
| Range | Depends on units. See Position Range for details. |
| Default Value |
42949672960 counts
|
| Data Type | Float |
| See Also | AXIS#.PL.FB |
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
GANTRY.PL.ERRFTHRESH |
300eh |
02h |
Signed32 |
Position |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
GANTRY.PL.ERRFTHRESH |
3001 |
BB9 |
Signed32 |
Read/Write |
Position |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
GANTRY.PL.ERRFTHRESH |
3001 |
Signed32 |
Read/Write |
Position |