REGEN.POWER
Description
This parameter reads regen resistor's calculated power, which is determined as follows:
(V2 / R) * DutyCycle
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Watt |
Range |
N/A |
Default Value |
N/A |
Data Type |
Integer |
See Also |
N/A |
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
---|---|---|---|---|---|---|---|
REGEN.POWER |
3007h |
02h |
Unsigned32 |
- |
- |
Read only |
Yes |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
REGEN.POWER |
2400 |
960 |
Unsigned32 |
Read Only |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
REGEN.POWER |
2400 |
Unsigned32 |
Read Only |
- |