REGEN.POWERFILTERED
Description
This parameter returns a filtered value of REGEN.POWER. A single order lowpass of 1/REGEN.TEXT Hz is applied to generate REGEN.POWERFILTERED.
If REGEN.POWERFILTERED exceeds the value of REGEN.WATTEXT, Fault 2010 (Regen overpower) will be generated.
This keyword may be recorded in the scope screen for analysis.
Example
REGEN.TEXT = 10 (seconds)
Lowpass Filter Frequence = 1/10 seconds = 0.1 Hz
REGEN.POWERFILTERED = REGEN.POWER * 0.1Hz lowpass
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
Watt |
|
Range |
0 to REGEN.WATTEXT |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
|
|---|---|---|---|---|---|---|---|
|
REGEN.POWERFILTERED |
3007h |
01h |
Unsigned32 |
- |
- |
Read only |
Yes |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
REGEN.POWERFILTERED |
2405 |
965 |
Unsigned32 |
Read Only |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.POWERFILTERED |
2405 |
Unsigned32 |
Read Only |
- |