VBUS.THREEPHASE

Description

This parameter indicates whether the AC line input is single or three phase, and whether phase loss detection is active.


  • Setting this parameter to 1/0 can enable/disable “phase loss” detection but it will not disable “power loss” detection.

“Power loss” condition is the condition where there is a sudden drop in the AC mains voltage. If this condition occurs, Fault 2014: AC input phase loss gets detected, inrush relay is opened, and the user must wait until VBUS.VALUE drops below VBUS.INRUSHOFF to clear the fault.

This mechanism is designed to protect the drive and fuse against potential damages due to sudden drops in the AC mains voltage.

Examples

Usage

If the parameter is set to 0, the drive assumes that the AC line input is single phase, and phase loss detection is turned off.

If the parameter is set to 1, the drive assumes that the AC line input is three phase, and phase loss detection is turned on. If the drive detects a phase loss condition and an axis is enabled, it throws Fault 2014: AC input phase loss on each axis.

Code

--> VBUS.THREEPHASE 1
--> DRV.FAULTS
1-2014: AC input phase loss.
2-2014: AC input phase loss.


--> VBUS.THREEPHASE 0
--> DRV.FAULTS
No faults active

Context

For more information on DC bus protection, refer to Power View and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 (single phase) to 1 (three phase)
Default Value 1 (three phase)
Data Type Integer
See Also VBUS.VALUE

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

VBUS.THREEPHASE

300ah

09h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.THREEPHASE

2509

9CD

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.THREEPHASE

2509

Unsigned8

Read/Write

-