VBUS.UVFTHRESH

Description

This parameter is the DC bus undervoltage fault threshold. When the measured DC bus voltage falls below the threshold, an undervoltage fault is thrown for each enabled axis.

Examples

Usage

The drive configures the minimum, maximum, and default values for this parameter based on power electronics ratings.

When an axis is enabled, and the measured DC bus voltage VBUS.VALUE is less than VBUS.UVFTHRESH, the drive throws Fault 2007: Bus under voltage.

When an axis is disabled and VBUS.VALUE is less than VBUS.UVTHRESH, the drive prevents the axis from enabling.

Code

The following example demonstrates the DC bus undervoltage fault check when Axis 1 is enabled and Axis 2 is disabled. The fault is reported on Axis 1 only.

--> VBUS.UVFTHRESH 100
--> VBUS.UVFTHRESH
100 [Vdc]
--> VBUS.VALUE
162.297 [Vdc]
--> AXIS1.EN
--> AXIS1.ACTIVE
1
--> AXIS2.ACTIVE
0



--> VBUS.VALUE
96.895 [Vdc]
--> AXIS1.ACTIVE
0
--> DRV.FAULTS
1-2007: Bus under voltage.

Context

For more information on DC bus voltage protection, refer to Power View and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Vdc
Range Dependent on drive model
Default Value Dependent on drive model
Data Type Integer
See Also VBUS.VALUE, VBUS.UVWTHRESH

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

VBUS.UVFTHRESH

300ah

02h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

VBUS.UVFTHRESH

2510

9CE

Unsigned16

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

VBUS.UVFTHRESH

2510

Unsigned16

Read/Write

-