| 0 |
No source |
Default value of no specified source |
N?A |
| 1 |
Mains ready |
This digital source goes high when the bus voltage is available to the drive. It does not take any ID or parameters. |
Digital |
| 2 |
Digital Input |
This digital source corresponds to a DIN. It takes an ID. |
Digital |
| 3 |
Digital DIO (Bidirectional) |
This digital source corresponds to DIO. It takes an ID. |
Digital |
| 4 |
Velocity Feedback |
This analog source holds the value of AXIS#.VL.FB
. It takes an axis ID. |
Analog |
| 5 |
Axis Faulted |
This digital source goes high when a fault exists on an axis. It takes an axis ID. |
Digital |
| 6 |
Home Complete |
This digital source is high when a Home operation is completed on an axis. It takes an axis ID. |
Digital |
| 7 |
Motion Task in Position |
This digital source is high when on an axis specified by the axis ID, a MotionTask specified by Source Parameter, has reached its position. It takes both ID and parameter. |
Digital |
| 8 |
Controlled Stop Active |
This digital source is high when a Controlled Stop is active on an axis. It takes an axis ID. |
Digital |
| 9 |
Software Limit |
This digital source is high when a software limit on an axis is reached. It takes an axis ID. |
Digital |
| 10 |
MT Not Running |
This digital source is high if, on the axis specified by the source ID, either the Motion Task specified by the source parameter has stopped running (i.e. AXIS#.MT.RUNNING for that task went from 1 to 0) or, if the source parameter is set to -1, all Motion Tasks have stopped running (i.e. AXIS#.MT.RUNNINGTASK went from any other value to -1). This source does not check whether the actual position has reached the Motion Task’s target position. |
Digital |
| 11 |
Position Error, Absolute |
This analog source holds the value of AXIS#.PL.ERR
. It takes an axis ID. |
Analog |
| 12 |
Axis Enabled |
This digital source holds the value of AXIS#.ACTIVE . It takes an axis ID. |
Digital |
| 13 |
Analog Input |
This analog source holds the value of AIN#.VALUE. It takes as Source ID, the ID of AIN. |
Analog |
| 14 |
Current Command |
This analog source holds the value of AXIS#.IL.CMD . It takes an axis ID. |
Analog |
| 15 |
Velocity Error |
This analog source holds the value of AXIS#.VL.ERR
. It takes an axis ID. |
Analog |
| 16 |
Velocity Command |
This analog source holds the value of AXIS#.VL.CMD. It takes an axis ID. |
Analog |
| 17 |
Position Feedback |
This analog source holds the value AXIS#.PL.FB
. It takes an axis ID. |
Analog |
| 18 |
Axis Disable Immediately |
This digital source goes High if the axis disables when a fault is generated with a fault reaction of either “Disable power stage” or “Dynamic braking”. Refer to the Reaction column in Faults and Warning Messages for more information. |
Digital |
| 19 |
Brake State |
This digital source holds the value of BRAKE#.STATE. It takes a Brake ID. |
Digital |
| 20 |
Ready to Operate (RTO/BTB) |
This digital source goes High when the drive/axis is ready to operate, i.e., the power stage is ready and there are no axis faults. It can default to an ID of 0 for the entire drive or take an axis ID. |
Digital |
| 21 |
Compare Digital Inputs |
This bit-mapped source shows the value of all the DINs and DIOs compared with a mask which is settable with UI. |
Digital |
| 22 |
Feedback Fault |
This source holds the value of FB#.FAULTBITS. It takes a Feedback ID. |
Digital |
| 23 |
User Variable |
This source holds the value of USER.INT#. It takes an ID. |
Analog |
| 24 |
Action Row Running |
This digital source indicates if an Action Row is running, i.e. if the task is being executed (see ACTION.RUNNING). It takes an Action Row ID. |
Digital |
| 25 |
Current Feedback |
This analog source holds the value of AXIS#.IL.FB . It takes an axis ID. |
Analog |
| 26 |
Recordable Parameter |
This allows an action to be triggered by using any Recordable Parameter. When selected, the Source Text window now accepts an array parameter keyword and index. 26 – Recordable Parameter |
Analog |
| 27 |
Drive Initialized |
This digital source goes high when the drive has finished initialization after booting. |
Digital |
| 28 |
Move Complete |
This digital source is high if, on the axis specified by the source ID, either the motion task specified by the source parameter has stopped running (i.e. AXIS#.MT.RUNNING for that task went from 1 to 0) and the actual position is within AXIS#.SETTLE.P around the motion task’s target position or, if the source parameter is set to -1, all motion tasks have stopped running (i.e. AXIS#.MT.RUNNINGTASK went from any other value to -1) and the actual position is within AXIS#.SETTLE.P around the last motion task’s target position. It will only go low when the motion task is started again, not if the actual position is no longer within AXIS#.SETTLE.P around the target position. |
Digital |
| 200 |
Safe Input |
This digital source holds the value of a SIN (Safety Digital Input). It takes the SIN ID. |
Digital |
| 201 |
Safe Dual Input |
This digital source holds the value of a DUAL (Dual Safety Digital Input). It takes the SIN DUAL ID. |
Digital |
| 202 |
Safe Output |
This digital source holds the value of a SOUT (Safety Digital Output). It takes the SOUT ID. |
Digital |
| 203 |
Safe Dual Output |
This digital source holds the value of a SOUT DUAL (Dual Safety Digital Output). It takes the SOUT DUAL ID. |
Digital |
| 204 |
STO Active |
This digital source holds the value of STO Active. It takes an Axis ID. |
Digital |
| 205 |
SS1 Active |
This digital source holds the value of SS1 Active. It takes an Axis ID and an Instance ID. |
Digital |
| 206 |
SS2 Active |
This digital source holds the value of SS2 Active. It takes an Axis ID and an Instance ID. |
Digital |
| 207 |
SOS Active |
This digital source holds the value of SOS Active. It takes an Axis ID and an Instance ID. |
Digital |
| 208 |
SBC Active |
This digital source holds the value of SBC Active. It takes an Axis ID. |
Digital |
| 209 |
SLS Active |
This digital source holds the value of SLS Active. It takes an Axis ID and an Instance ID. |
Digital |
| 210 |
SSM in Range |
This digital source holds the value of SSM in Range. It takes an Axis ID and an Instance ID. |
Digital |
| 211 |
SSR Active |
This digital source holds the value of SSR Active. It takes an Axis ID and an Instance ID. |
Digital |
| 212 |
SDIn in Motion |
This digital source holds the value of SDIn in Motion. It takes an Axis ID. |
Digital |
| 213 |
SDIp in Motion |
This digital source holds the value of SDIp in Motion. It takes an Axis ID. |
Digital |
| 214 |
SLA Active |
This digital source holds the value of SLA Active. It takes an Axis ID. |
Digital |
| 215 |
SAR Active |
This digital source holds the value of SAR Active. It takes an Axis ID and an Instance ID. |
Digital |
| 216 |
SLI Active |
This digital source holds the value of SLI Active. It takes an Axis ID and an Instance ID. |
Digital |
| 217 |
SLP Active |
This digital source holds the value of SLP Active. It takes an Axis ID and an Instance ID. |
Digital |
| 218 |
SCA in Range |
This digital source holds the value of SCA in Range. It takes an Axis ID and an Instance ID. |
Digital |