Coordinated Motion Terminology
|
Term |
Definition |
|---|---|
|
ACS |
Axes Coordinate System. The system of coordinates related to the physical motors and the single movements caused by the single drives. |
|
Blending |
A way that consecutive function blocks cooperate in the transition from the first to the next. |
|
Contour Curve |
Inserted curve that modifies the original path. It is the resulting curve after blending. |
|
Coordinate system |
The reference system in which a coordinate or path is described. |
|
Corner deviation |
The shortest distance between the programmed corner point and the contour curve. |
|
Corner distance |
Distance of the start point of the contour curve to the programmed target point. |
|
Direction |
The orientation components of a vector in space. This is different from the MC_Direction input as used in part 1. |
|
Drive |
A unit controlling a motor using the current and timing in its coils. |
|
Group-FB |
The set of function blocks that can work on a group of axes. |
|
MCS |
Machine Coordinate System.
Sometimes called “World Coordinate System” or “Base Coordinate System”.
|
|
Motor |
An actuator |
|
Orientation |
The rotational components of a vector in space. |
|
Path |
Set of continuous positions and orientation information in multi-dimensional space. Geometrical description of a space curve that the TCP of an axesgroup moves along. |
|
PathData |
Description of a path which can include additional information like velocity and acceleration. |
|
PCS |
Product Coordinate System or Program Coordinate System.
|
|
Position |
Position means a point in space which is described by different coordinates.
In ACS there can be even more than six coordinates.
|
|
Scara |
A special kinematic for robot or handling applications. |
|
Speed |
Speed is the absolute value of the velocity without direction. |
|
Synchronization |
Combines an axis or axes group (as slave) with an axis as master.
|
|
TCP |
Tool Center Point.
|
|
Tracking |
Is characterized by an axis group that follows with its movement the movement of another axis group. |
|
Trajectory |
Time dependent description of the path the TCP of an axes group moves along.
|
|
Velocity |
For a group of axes this means:
|