DRV.DBILIMIT
Description
This parameter sets the maximum amplitude of the current for dynamic braking.
Example
Setting DRV.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.
General Information
|
Type |
NV Parameter |
|
Units |
Arms |
|
Range |
0 to minimum of drive peak current (DRV.IPEAK) and motor peak current (MOTOR.IPEAK). |
|
Default Value |
Minimum of drive continuous current (DRV.ICONT) and motor continuous current (MOTOR.ICONT). |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
| Index/Subindex | Object Start Version |
|---|---|
|
3444h/0 |
M_01-00-00-000 |