DRV.EMUEZOFFSET
Description
When emulated encoder output (EEO) multiturn is selected (DRV.EMUEMODE=1), this parameter is used by itself to define the position if the Z pulse within one revolution.When the primary feedback position (within a revolution) equals this value, an index pulse will output. Also, if DRV.EMUEMODE=1 then this parameter is used in conjunction with DRV.EMUEMTURN.
When the EEO is configured to generate an absolute index pulse (DRV.EMUEMODE is 2, 7 or 9) this parameter and DRV.EMUEZOFFSET define the location of the Z pulse. DRV.EMUEMTURN is used to define which turn of the position range the Z pulse is located and DRV.EMUEZOFFSET is used to define the position of the Z pulse within one revolution.
Note: If you are using multi-turn or single tune absolute feedback devices the Z pulse from generated by the EEO will always be aligned with the same mechanical position of the of the primary feedback position. If you are using an incremental feedback device
A process whereby some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position then the origin of the primary feedback is not at the same mechanical position each time the drive powers up.
General Information
|
Type |
R/W Parameter |
|
Units |
1/65536 rev |
|
Range |
0 to 65535 rev |
|
Default Value |
0 rev |
|
Data Type |
Integer |
|
Start Version |
M_01-00-00-000 |