DRV.WARNINGS

Description

DRV.WARNINGS returns a list of all currently active warnings in the system.

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-00-00-000

Variant Supported
MKD EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs Yes
AKD-N Yes
MKD-N Yes
MKD-C Yes