MOTOR.NAME
Description
This parameter is used to set the motor name.
-
- This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
20 chars |
|
Default Value |
N/A |
|
Data Type |
String |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Related Topics