MOTOR.PHASE

Description

This parameter sets the motor phase.


  • If MOTOR.AUTOSET = 1 and FB1.MEMVER > 0.01, this parameter will be automatically configured for Kollmorgen motors.


  • When loading a parameter file to a new device, if MOTOR.AUTOSET = 0 then motor parameters should be checked to make sure they are properly configured for the motor on the new device.

General Information

Type

NV Parameter

Units

Electrical degrees

Range

0 to 360°

Default Value

0°

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen
Index/Subindex Object Start Version

359Ch/0

M_01-00-00-000

Related Topics

Motor View