MOTOR.R

Description

MOTOR.R sets the stator winding resistance phase-to-phase in ohms.

General Information

Type

NV Parameter

Units

Ω

Range

0.001 to 650 Ω

Default Value

10 Ω

Data Type

Float

See Also

N/A

Start Version

M_01-00-00-000

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen ]
Index/Subindex Object Start Version

3456h/0

M_01-00-00-000

Related Topics

Motor View