Alias Definitions
- An alias is a unique
identifier used in programs to replace another text.
- Definitions are typically used to replace a constant expression and facilitate the maintenance of programs.
- See usage in Use the Defines List for more information.
There are three levels of definitions:
- Common to all the projects present on your machine
- Global to all programs within your project
- Local to one program
Local definitions are edited together with the corresponding program.
- Definitions are entered in a text editor.
- Each definition must be entered on one line of text following this syntax:
#define Identifier Equivalence (* comments *)
Examples
#define OFF FALSE (* redefinition of FALSE constant *) #define PI 3.14 (* numerical constant *) #define ALARM (bLevel > 100) (* complex expression *)
- You can use a definition within the contents of another definition.
- The definition used in the other one must be declared first.
Example
#define PI 3.14 #define TWOPI (PI * 2.0)
- A definition can be empty
Example
#define CONDITION
The defined word can be used for directing the Conditional Compiling directives.
-
-
You can enter #define lines directly in the source code of programs in IL
"Instruction List"
This is a low-level language and resembles assembly or ST
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal languages.
The use of definitions can disturb the program monitoring and make error reports more complex. It is recommended to restrict the use of definitions to simple expressions that do not risk creating a misunderstanding when reading or debugging a program.
|
Word |
Description |
|---|---|
|
_DATE_ |
Date stamp of compiling expressed as a string constant expression. Format is: Year/Month/Day-Hours-Minutes. |
|
_MACHINE_ |
Name of the machine where compiling is run, expressed as a string constant expression. |
|
_USER_ |
Name of the user where compiling is run, expressed as a string constant expression. |
Example
This ST program sets variables declared as STRING(255):
strDate := __DATE__; strMachine := __MACHINE__; strUser := __USER__; strProject := __APPNAME__; Result: strDate is '2007/11/25-10:45' strMachine is 'LaptopJX' strUser is 'John'