FBD Corners
Corners are used to force the routing of connection lines, as the FBD
"Function Block Diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks editor
imposes a default routing only between two pins or user-defined corners.
All variable symbols and constant expressions are entered in FBD diagrams using small boxes.
Select the Insert Corner button in the FBD toolbar to insert a corner on a line:
![]()
Insert corner: In this mode, the mouse is used to insert a user-defined corner on a line.
- Drag a new line from an output pin to an empty space.
- In this case, the editor automatically finishes the line with a user-defined corner.
- Continue drawing the connection to the desired pin and force the routing while you are drawing the line.
- Corners can then be selected and moved to change the routing of existing lines.