AS-interface Functions
|
Description |
|
|---|---|
|
ASiReadPI |
Read actual parameters of an AS-i slave. |
|
ASiReadPP |
Read permanent parameters of an AS-i slave. |
|
ASiSendParam |
Send parameters to an AS-i slave. |
|
ASiStorePI |
Store actual parameters as permanent parameters. |
|
ASiWritePP |
Write permanent parameters of an AS-i slave. |
-
-
AS-i networking may be not available on some targets.
See the OEM
"Original equipment manufacturer"
A term that refers to containment-based re-branding, namely where one company uses a component of another company within its product, or sells the product of another company under its own brand. OEM refers to the company that originally manufactured the product instructions for more information.
Interface
Params := ASiReadPP (Master, Slave);
bOK := ASiWritePP (Master, Slave, Params);
bOK := ASiSendParam (Master, Slave, Params);
Params := ASiReadPI (Master, Slave);
bOK := ASiStorePI (Master);
Arguments
Master : DINT Index of the AS-i master (1..N) such as shown in configuration.
Slave : DINT Address of the AS-i slave (1..32 / 33..63).
Params : DINT Value of AS-i parameters.
bOK : BOOL TRUE if successful.