Bookmarks
- Insert bookmarks anywhere in a document.
- Use them to jump from one bookmark to another with a single command for browsing the document.
- Bookmarks are supported in all program editors plus the Variable editor.
These are the available commands for using bookmarks:
|
Command |
Description |
|---|---|
|
Ctrl + F2 |
Toggle the bookmark at the current position. |
|
Shift + F2 |
Go to the next bookmark. |
According to the type of document, the possible locations for a bookmark are:
- In the FBD
"Function Block Diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks editor, a bookmark is placed on any FBD object (not on a line). - In the FFLD
"Free Form Ladder Diagram" editor, a bookmark is placed on a rung header. - In the SFC
"Sequential Function Chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions editor, a bookmark is placed on an SFC symbol (step, transition, jump...). - In the text editor, a bookmark is placed on a line of text.
- In the Variable editor, a bookmark is placed on any line of the grid (variable or group).
-
-
Bookmarks are valid only while the editing window is open.
They are not stored in the document when the window is closed.