Download AKD PDMM Drive Firmware

Component

Title

Download Link

800MHz AKD PDMM Drive FW

AKD PDMM Servo Drive Firmware

(AKD-M-MCEC-[firmware version])

1.2GHz AKD PDMM Drive FW

AKD PDMM Servo Drive Firmware

(AKD-M-M1EC-[firmware version])

Update the AKD PDMM Drive Firmware with KAS-IDE

  1. In the toolbar, deactivate the Online Configuration Mode.
  2. Select the drives requiring the same firmware version to be updated.

    • The firmware download is limited to 16 drives at a time.

  3. Click the Upgrade Firmware button.

    • Warning dialogs may appear at this point.
      These warnings include important information about preventing damage to the drives.

  4. Browse to the new AKD/AKD2G firmware file.
    See the Release Notes for the latest supported firmware.
  5. Click Open to start the updating procedure.