HMI - Graphic Operator Interface

This is a list of HMI available component:

HMI Part Number

Description

KVB

Manual

AKI-CDC-MOD-21T-000

Graphical Display 21.5" TFT LCD, Touchscreen

v2.0

AKI-CDC-MOD-15T-000

Graphical Display 15.4" TFT LCD, Touchscreen

v2.0

AKI-CDC-MOD-12T-000

Graphical Display 12.1" TFT LCD, Touchscreen

v2.0

AKI2G-CDA-MOD-07T-000

Graphical Display 5" TFT LCD, Touchscreen

v2.20

AKI2G-CDA-MOD-05T-000

Graphical Display 7" TFT LCD, Touchscreen

v2.20

AKI2G-CDB-MOD-12T-000

Graphical Display 12" TFT LCD, Touchscreen

v2.20

AKI2G-CDB-MOD-07T-000

Graphical Display 7" TFT LCD, Touchscreen

v2.20

See the Kollmorgen Support Network for specifications and Technical Manuals.

Concept Link IconSee Also