eipWriteAttr
Function Block - Sends an explicit message (UCMM) to an EtherNet/IP adapter to write a single CIP attribute.
Inputs
|
Input |
Data Type |
Range |
Unit |
Default |
Description |
|---|---|---|---|---|---|
|
Attr |
UINT |
|
|
|
Identifier of the CIP attribute. |
|
Class |
UINT |
|
|
|
Class identifier of the CIP object. |
|
Data |
array of UINT |
Buffer containing the data to write. |
|||
|
Inst |
UINT |
|
|
|
Instance identifier of the CIP object. |
|
SrvIP |
STRING |
|
|
|
IP address of the server (adapter) (e.g., configured in the EtherNet/IP Scanner configuration). |
|
Size |
UINT |
Number of bytes to write. Cannot exceed 450 bytes. |
|||
|
Snd |
BOOL |
FALSE, TRUE |
N/A |
No default |
A rising edge on this input starts the exchange. The DONE output signals the end of exchange. |
Outputs
|
Output |
Data Type |
Range |
Unit |
Description |
|---|---|---|---|---|
|
Done |
BOOL |
FALSE, TRUE |
N/A |
This output is TRUE during one cycle when the exchange is finished, whether the exchange succeeded or failed. Warning: This output can be TRUE just after the call to block when starting a new exchange in case of invalid parameters. |
|
EmErr |
UINT |
|
|
In case of a UCMM error, this is the CIP general status error code. |
|
EmErrExt |
UINT |
|
|
In case of a UCMM error, this is the CIP extended status error code. |
|
Err |
UINT |
|
|
Main error report. Can be one of these values: |
|
RcvSize |
UINT |
|
|
Actual size of the CIP attribute answered by the server. If this size is greater than the size of the DATA input array, it indicates the value was truncated. |
Remarks
- The CIP instance number can be 16-bits [1...65535].
- The servers (adapters) accessed by this block must be configured in the EtherNet/IP Scanner fieldbus configuration.
- Only one explicit message (read or write) can be sent at one time to the same server.
- If another message is pending you receive the error report 3 (busy) after calling the block to start a new exchange.
- Consider SerializeIn and SerializeOut functions for extracting data from the read buffer.
FBD Language Example
Not available.
FFLD Language Example
Not available.
IL Language Example
Not available.
ST Language Example
// used variables
// Inst_eipWriteAttr : eipWriteAttr ;
// bWrite : BOOL ; (* request for WRITE *)
// DataWrite : ARRAY [0 .. 15] OF USINT; (* written data *)
// uiSizeWrite : UINT := UINT#16 ; (* number of bytes to read *)
// Server identification and CIP things
#define SRVIP '192.168.33.21'
#define CLASSID UINT#100
#define INSTID_WRITE UINT#2
#define ATTRID UINT#3
/////////////////////////////////////////////////////////////////////////////////////////
// requested WRITE command
if bWrite then
Inst_eipWriteAttr (bWrite, SRVIP, CLASSID, INSTID_WRITE, ATTRID,
uiSizeWrite, DataWrite);
end_if;
// WRITE answer here ?
if Inst_eipWriteAttr.Done then
// check answer
if Inst_eipWriteAttr.Err = 0 then
printf ('WRITE ok');
else
printf ('WRITE Error %lu - (UCMM Error %lu, %lu)',
any_to_dint (Inst_eipWriteAttr.Err),
any_to_dint (Inst_eipWriteAttr.EmErr),
any_to_dint (Inst_eipWriteAttr.EmErrExt));
end_if;
// reset WRITE command and block input
Inst_eipWriteAttr (false, SRVIP, CLASSID, INSTID_WRITE, ATTRID,
uiSizeWrite, DataWrite);
bWrite := false;
end_if;
See Also