USB Flash Drive Path Conventions
Access to the USB flash drive memory requires that a valid USB flash drive label be used at the beginning of the path, followed by the relative path to the USB flash drive.
(Valid USB Flash Drive Label)/(Relative Path)
- A valid USB flash drive relative path starts with //, /, \\, or \.
- This is immediately followed by usbflash which is followed by \ or /.
- This path label is case insensitive.
The usbflash folder is created inside the userdata folder to maintain compatibility with the Simulator.
File access points to userdata/usbflash when a PCMM2G usbflash path is used on the Simulator.
Valid Paths
|
Valid Paths |
Notes |
|---|---|
|
//usbflash/file1 |
|
|
\usbflash/dir1/file1 |
dir1 must have been already created. |
|
/usbflash/dir1/file1 |
dir1 must have been already created. |
|
//usbflash\file1 |
|
Invalid Paths
|
Invalid Paths |
Invalid Reason |
|---|---|
|
///usbflash/file1 |
Started with more than two forward or two backward slashes. |
|
/\usbflash/dir1/file1 |
Started with one forward and one backward slash. |
|
/usbflashdir1/file1 |
No forward or backward slash. |
|
/ubflash1/dir1/file1 |
Invalid label. |
See Also